cancel
Showing results for 
Search instead for 
Did you mean: 

EEPROM ST 950406 replacement

Tom6
Associate

Hi,

any help or information to find the data sheet and to determine an available replacement type for an obsolete EEPROM chip from ST marked 950406 would be highly appreciated.

A picture of the chip is attached.

The defective EEPROM chip 950406 comes from a Landis & Staefa heating controller, year of manufacture of the controller was +- 2002.

Thanks in advance and best regards.

2 REPLIES 2

ST95040M6TR SOP8

EEPROM 5.5V 4K (512x8)

https://community.st.com/t5/other-hardware/hi-i-don-t-want-to-know-if-the-95042u3-is-simply-an-95040-i-don/td-p/210432

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Peter BENSCH
ST Employee

@Tom6 You could try the M95040-RMN6TP or the M95040-FMN6TP. The ST950406 can only be operated with 5V, but the alternatives can be operated from 1.7V or 1.8V up to and including 5V.

Hope that helps?

Good luck!
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.