2005-04-17 08:27 PM
2005-04-07 01:08 AM
Hello,
I don't know how to use the arithmetic functions of the DSP library for floating point operations. Is there a other way to realize floating point operations by the DSP library? A software problem occurs when a floating point value in the C code is multiplied by 0 (without the DSP livbrary): then there is an exception, which is triggered by the ST10. Why is this happening? Thank you for your support.2005-04-14 11:04 PM
Hello,
The DSP library is only handling fixed point variables. For floating point, for many functions there are either algorithms available, either tools to generate ANSI C code that can be compiled with a ST10 toolchain. For the handling of the exceptions in floating point libraries, this is related to the compiler. There is an option to check or not for these exceptions.2005-04-14 11:56 PM
Hello,
I have to optimize a self-written C function, which uses floating point variables. Is this possible with the MAC unit of the ST10f269? How can I involve the MAC unit? Or are there other possibilities? Where can I find these tools that generate ANSI C code for floating point operations? Is this code then already optimized? Thank you for the information. :-)2005-04-17 08:27 PM
Quote:
How can I involve the MAC unit?
With the Cosmic ST10 compiler, there is at least one way to ''force'' the use of the MAC with C Code. However I don't think that floating point stuff is the best candidate to achieve significant optimization when using the MAC. If you want mor details you can contact me offline. Regards, Luca (Cosmic)