2007-09-14 01:18 AM
Debug error when booted from bank1
2011-05-17 12:46 AM
Hi all.
I want to load an iap bootloader to bank1 and bootloader will load application to bank0.A few days ago i couldn't boot from bank1. Now it boots from bank1. I found in forum STR91xCFG_Bank1.s file that set CSX bit.If i use this file i can boot from bank1.What for is this file?Who set CSX bit with using this file?Is it jtag? But when i want to debug Keil gives ERROR: Memory Missmatch ! Address : 0x00520000 Value = 0x33 Expected = 0x00 How can Value at 0x00520000 be 0x33.Who did write there? In STR91xCFG_Bank1.s file i set CSX bit(first bit at 0x00520006) My aim is a bootloader occupied on bank1 that get application from uart and load bank0.Is there any one who has sample project? Regards... Mehmet