cancel
Showing results for 
Search instead for 
Did you mean: 

Choices of C Compilers for ST7F part?

mtignor
Associate II
Posted on April 16, 2006 at 20:40

Choices of C Compilers for ST7F part?

10 REPLIES 10
mtignor
Associate II
Posted on February 06, 2006 at 17:18

I am looking at the alternatives for ST7F tools for C compiler and debug. I have a package from Cosmic. Are the any other choices? I see Metrowerks listed in web pages at Softecmicro. But I can't find much more info than this.

Are these the only two choices? - thanks, Mike

wolfgang2399
Associate II
Posted on February 07, 2006 at 06:09

Hi Mike,

I've never heard of any other C-Compiler for ST7 than Cosmic and Metrowerks.

I use the Metrowerks and the STVD7 (visual develop) from STMicro and I am comfortable with both of them.

You can download the STVD7 from the

http://mcu.st.com/mcu/modules.php?name=mcu&file=familiesdocs&FAM=15

and use it for free. It is a quite practical tool.

You may use the STVD7 with the Cosmic as well.

Regards

WoRo

Viktor POHORELY
ST Employee
Posted on February 07, 2006 at 08:32

I will strongly recommend to use Cosmic in combination with STVD7 toolchain.

sylv1laurent
Associate II
Posted on February 08, 2006 at 17:18

Hi Mike,

I have developed an IP stack on ST7F321 with C-Cosmic and several routine in asm with an EMU3.

This emulator is very good to develop and debug complex application.

I have had lot of problems with cosmic C to integrate C and ASM, especialy for routine parameter and variable declaration.

Regards

Sly

luter
Associate II
Posted on February 09, 2006 at 03:39

Hi.

I use Cosmic since 1 year and I am satisfied. I did not have any big problems due to compiler.

luca239955_st
Associate III
Posted on February 09, 2006 at 06:59

Quote:

....

I have had lot of problems with cosmic C to integrate C and ASM, especialy for routine parameter and variable declaration.

What problems?

Just curious.

Regards,

Luca (Cosmic)

wolfgang2399
Associate II
Posted on February 09, 2006 at 07:04

Hi Setler,

I've never had any problems with Cosmic using the STVD7 - but I don't have any after I've changed to the Metrowerks C-compiler.

So why do you ''strongly recommend'' to use the Cosmic compiler???

Regards

WoRo

xpcommon
Associate
Posted on February 09, 2006 at 16:29

Hi new here, i would rather prefer STVD7

sisto
Associate II
Posted on April 15, 2006 at 14:09

I will strongly recommend to use Cosmic in combination with STVD7 toolchain.

I vote at all !!

I use Cosmic ''C'' compiler from about 4 years without any problem... You can believe to me !

So You can just investigate if You are using it correctly.

The Cosmic support service is very efficient to help You about any problem You have.

Sixtus