2020-10-07 03:40 PM
Hi,
I am using M34E04 I2C EEPROM
read and write access works fine but I cannot enable write protection
I have verified the WC pin is in the right state (logic 1) but I can still write to the device at this mode
Any tip?
Regards
Assaf
2020-10-13 05:50 AM
2020-10-14 02:35 PM
Hi,
I am not intending to use the SW commands for activating the write protect
I am only interested in the HW write protect using the WC pin
Per data sheet setting the WC pin has higher priority over the SW commands
Also the SW commands require VHV (high voltage) which I would like to avoid
Is there any limitation with using the WC pin?
Regards
Assaf
2020-10-20 06:49 AM
hello,
yes WC has higher priority. With HW write protect enabled , the memory array is protected against write command.
(warning not valable for SWP,CWP command)
BR
EEPROM Team suPPort