cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeProgrammer 2.15.0 released

Aziz BRIGUI
ST Employee

STM32CubeProgrammer v2.15.0 release information

New features:
• Added the NOR flash memory and OTP fuse programming via USB and UART using OpenBootloader for the STM32MP13xx microprocessors

• Added the support for the PMIC programming via UART for the STM32MP15xx microprocessors

• Added limited FASTROM support

• Added the automatic determination of the stack install address for the STM32WB series and STM32WB0 series

Refer to the STM32CubeProgrammer software description user manual (UM2237) for details.

Fixed issues:
110598 [STM32CubeProg][STM32WB] Incorrect installation address when the RF stack is already in place.

124075 [GUI][Device memory] Request to remove the partitions view from Device memory.

140915 [STM32L0][EEPROM] Error message when erasing the EEPROM via the ST-LINK interface.

145199 [STM32CubeProg-FUS] [STM32WB15xx] Missing the wireless stack version.

150022 [STM32F0][STM32CubeProg] Confusing naming and use of nWRP.

150428 [STM32WB][DFU] The [Start Wireless Stack] button is grayed in DFU mode.

153021 The STM32WB firmware upgrade of a large stack shows an error while it is passed.

153419 [Option bytes][Device_ID = 0x480] FLASH_OTPBL_PRG is missing from the OB list.

155082 Wrong RSS version displayed on STM32CubeProgrammer/CLI.

155918 [STM32CubeProg] The connection error popup cannot be closed using the [X] close button.

158082 [STM32L4][DBANK] Wrong sector size when DBANK is disabled.

158507 [DATABASE][OB] Missing nDBOOT OB for 1‑Mbit targets.

159061 [Device_ID = 0x467][DATABASE] Remove testing on dual bank for the 128‑Kbit flash memory size.

159172 [STM32CubeProg][API] Bank number is always zero due to a wrong name size in the DeviceDataStruct ure.h file: 32 instead of 64.

159589 Error returned by TPC when used embedded in STM32CubeMX.

160062 [DATABASE][OB] Write protection option bytes are not shown via the bootloader interface.

161652 [SFI] Instability on STM32U5 microcontrollers with official release 2.14.0.

Known problems and limitations:

Automatic update from STM32CubeProgrammer 2.14 to STM32CubeProgrammer 2.15 is not possible. It is recommended to install the new version manually.

Refer to the STM32CubeProgrammer Release note (RN0109) for further details.

Download Link:

https://www.st.com/en/development-tools/stm32cubeprog.html


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
0 REPLIES 0