cancel
Showing results for 
Search instead for 
Did you mean: 

Can you propose me the alternative part of IGBT similar spec follow this table below?

amamam02989
Associate

I need to use IGBT for my new design. Can you propose me the alternative part of IGBT similar spec follow this table but surface mount?

Voltage - Collector Emitter Breakdown600 V
Current - Collector (Ic)23 A
Current - Collector Pulsed 92 A
Vce(on) (Max) @ Vge, Ic2.6V @ 15V, 12A
Power 75 W
Switching Energy115µJ (on), 135µJ (off)
Td (on/off) @ 25°C17ns/60ns
Operating Temperature-55°C to 150°C
1 REPLY 1
Peter BENSCH
ST Employee

Welcome @amamam02989, to the community!

you could have a look at the STGB20H65FB2.

Hope that helps?

Good luck!
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.