2023-10-30 10:01 PM
I need to use IGBT for my new design. Can you propose me the alternative part of IGBT similar spec follow this table but surface mount?
Voltage - Collector Emitter Breakdown | 600 V |
Current - Collector (Ic) | 23 A |
Current - Collector Pulsed | 92 A |
Vce(on) (Max) @ Vge, Ic | 2.6V @ 15V, 12A |
Power | 75 W |
Switching Energy | 115µJ (on), 135µJ (off) |
Td (on/off) @ 25°C | 17ns/60ns |
Operating Temperature | -55°C to 150°C |
2023-11-01 09:16 AM
Welcome @amamam02989, to the community!
you could have a look at the STGB20H65FB2.
Hope that helps?
Good luck!
/Peter