2008-06-17 07:03 AM
Can't programming my upsd3354DV with ULINK2 (Print version 2)
2011-05-17 02:52 AM
Last week my ULINK1 USB-JTAG Connector was broken.
Today I received a new ULINK2. But the new ULINK2 doesn't work. When I tried to programming my uPSD3354DV chip following error occurred: Erasing Flash... Erasing PLD/ACR... Programming Flash Block 0 (FS0) Flash Programming Error in Block: 0x00000 - 0x00039 ***Error: Programming failed The firmware version of the ULINK2 is V1.30. The Softwareversion of Keil uVision is V3.60. For the Flash Programming I use the St -uPSD ULINK Driver. (UL2UPSD.DLL V2.63) With another ULINK2 (Print Version 1) I bought last year I can download a program without problems to the uPSD3354. I already tried a second ULINK2 (Print Version 2) because i believed the first ULINK2 was broken. But both ULINK2 doesn't work. Do you have any suggestions for solving the problem?2011-05-17 02:52 AM