2005-09-06 01:47 PM
Can't boot Linux with the DiskOnChip 2000 installed?
2005-09-05 05:41 PM
The Linux system can't boot with the DiskOnChip 2000 installed. But it can boot normally without the DOC. When the bootstrapping begins, the following error messages prompts,
Lilo Errors 0x40 I don't know the exact reason. If you know about the error. Please help me. Thank you!2005-09-06 05:59 AM
So, the problem of boot occurs only with the DOC!
Did you configured the DiskOnChip as a bootable disk for the linux? In any case I have attached the Installation manual for the DiskOnChip2000 with Linux to verify again your configuration. ________________ Attachments : APP21.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtsO&d=%2Fa%2F0X0000000aYE%2FhlkNmZdee00d9Y_RaMfxHzoPt5FcZVMHhNsoXZ9OWaM&asPdf=false2005-09-06 01:47 PM
Yes, perhaps it's the problem. But I can boot the linux from the DOC without CF-Card installed.
Thank you for your suggestion. I'll read the manual very carefully.