Posted on September 06, 2005 at 22:47Yes, perhaps it's the problem. But I can boot the linux from the DOC without CF-Card installed. Thank you for your suggestion. I'll read the manual very carefully.
Posted on September 06, 2005 at 09:10When I execute expr command in a customized linux system, it prompt that expr command cann't be found. But the bash is running properly. And expr is a builtin command in bash. Why?
Posted on September 06, 2005 at 02:41The Linux system can't boot with the DiskOnChip 2000 installed. But it can boot normally without the DOC. When the bootstrapping begins, the following error messages prompts, Lilo Errors 0x40 I don't know the exa...
Posted on September 03, 2005 at 06:55I run a customized linux system on stpc atlas, the kernel is 2.4.20, the filesystem is from redhat9.0. On bootstrapping, the system boots from Lilo perfectly well until it comes to the section shown in the attach...
Posted on June 28, 2005 at 08:32Hi, Does you know how to support hard disk on a Consumer-II board in WinCE 4.2? And how to use hive-based registry? Any hint will be helpful. Thanks!