2008-08-07 08:43 PM
Anglia IDEaliST and Olimex ARM-USB-TINY
2011-05-17 12:54 AM
Hi All,
I managed to work out a partial answer. IDEaliST generates a 'openocd.cfg' file automatically in the project root (I was looking in the IDEaliST install directory beforehand). Whenever the debugger gets started, a new 'openocd.cfg' file is generated and overwrites the old one. So hand editing this file is pointless. The way I got the debugger working was to untick ''AutoStart Debug Driver when Debugging'' in Debug options, and starting OpenOCD manually in a command prompt with the correct config file. I still haven't got the 'Program Flash...' facility going... [I might have a good look at Code::Blocks and see if I can get the tools integrated easier???] regards, Mykola2011-05-17 12:54 AM
Hi,
I am trying to get Anglia IDEaliST (IDE ver 1.61; Toolchain ver 1.62) with the Olimex ARM-USB-TINY. I downloaded the latest openocd (openocd-ftd2xx; svn 717) and managed to get the Jtag hardware recognised and the debugger working (Yagarto). I had to do one change and that was to change the PID from 0x0003 to 0x004, and keep VID as 0x15BA. PID of 0x0003 is for ARM-USB-OCD. Functioning configuration file attached. Now, looking at IDEaliST, there is an (older) version of openocd included. 'olimex-jtag' is available as a hardware option in the GUI, as is necessary. But beyond that, the GUI configuration is limiting. Unfortunately I cannot find any configuration file to manually adjust settings (PID, etc). Any assistance will be most appreciated. regards, Mykola2011-05-17 12:54 AM
Hi,
I am still getting a ''Hardware Setup Failed, Check Connections'' pop-up (title on pop-up is ''IDEaliST\Plugins\idestr9'') when trying to program the flash. Any ideas what the configuration should be? Any reasonable documentation for IDEaliST? regards, Mykola PS The reason I am posting here, is that this products has been referred to, and on person is developing for it????