2009-08-07 03:08 AM
ADC External Voltage Reference - ST6232
2004-05-11 12:58 AM
The ST6232 datasheet refers to a separate ''power supply'' for the ADC to be appplied on pins AVdd and AVss. Is this actually the PSU or the ADC reference voltage (as I think it is). Is the Power supply for the ADC actually derrived from Vdd and Vss of the MCU.
I'm planning to power the MCU from 5Vdc with a 2.5V precision reference to AVdd and AVss ............ will this work2004-06-10 12:12 AM
Hi,
The pin is for ADC power supply decoupling only. It is internally connected to the supply rail. This is detailled in the datasheet DO NOT connect a different supply, as you can imagine, bad things will happen!! hope this helps Simon2004-06-10 10:14 PM
The Data sheet says this:
''AV DD and AV SS . Power is supplied to the MCUA/D converter independently from the rest of the chip using these two pins.'' I'm really confused ??2009-08-07 03:08 AM
I am looking for ST62E32BF1 or ST62T32BB6
could help me? you have some piece? where can I buy them?