2006-06-08 03:33 AM
ADC connections if not used, RTC VBATT connection
2011-05-17 12:30 AM
Hello,
I'm working on a design with the 128 pin STR912FW44X6. I don't need to use the internal ADC(but I want to use GPIO Port 4 as general purpose I/Os). Are there any recommendations for connections to the pins AVSS, AVDD and AVREF ? I want to use the RTC but don't need to supply power to the RTC Unit when the main digital supplies (VDD and VDDQ) are switched off. Can I tie VBATT to GND oder are there other recommendations ? Thank you in advance, Sascha2011-05-17 12:30 AM
Hi Sascha,
I don't have the correct answer right now, I will ask and I will let you know rapidly. Best regards, STARM ;)2011-05-17 12:30 AM
Hi Sascha,
Please find the answers to your questions: 1- connect the AVDD, AVREF to VDDQ and AVSS to VSS 2- When not using battery for RTC, please connect the VBATT pin to VDDQ (do not connect to ground). Best Regards, STARM2011-05-17 12:30 AM
Thank you very much!