cancel
Showing results for 
Search instead for 
Did you mean: 

Disabling of "Generation application code"

MMont.15
Associate II

Hi,

I would like to say if it is possible to disable the automatic generation of the application code because it always overwrites what I change. For example, if I change something inside a driver file, when I compile, at first it automatically overwrites all the files by using the default files and then it compiles. Thanks for the help.

Marco

This discussion has been locked for participation. If you have a question, please start a new topic in order to ask your question
1 REPLY 1
Amel NASRI
ST Employee

Hello,

Could you please precise: is your question related to STM32CubeMX?

It is getting lost on the Community as there is no topic assigned.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.