cancel
Showing results for 
Search instead for 
Did you mean: 

Disabling of "Generation application code"

MMont.15
Associate II

Hi,

I would like to say if it is possible to disable the automatic generation of the application code because it always overwrites what I change. For example, if I change something inside a driver file, when I compile, at first it automatically overwrites all the files by using the default files and then it compiles. Thanks for the help.

Marco

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Amel NASRI
ST Employee

Hello,

Could you please precise: is your question related to STM32CubeMX?

It is getting lost on the Community as there is no topic assigned.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.