cancel
Showing results for 
Search instead for 
Did you mean: 

I am configuring the flexray controller.After setting the parameters, a RUN command is given which changes the POC_state from POC:ready to POC:startup. But further change of state to POC:normalactive is not observed.

RSeba.2
Associate III

The FlexRay cluster I have here consist of 2 FlexRay cold-start nodes and the third node, spc58ec mcu non-cold start node. Can anybody suggest what can go wrong ?

4 REPLIES 4
JLi.311
Associate II

I also want to use the FlexRay, Is this code write by yourself or transplant from other project?

Erwan YVIN
ST Employee

Hello Sebastian ,

Have you solved your issue ?

it could be due to the loss of synchronization with the network.

Best Regards

Erwan

RSeba.2
Associate III

Hello,

Yes. It has been resolved. The issue was with the MCR register's configuration. After correctly setting the MCR register, I reached the expected protocol state normal active.

Thanks and kind regards,

RSeba

Hello,

Currently I am doing the transmit buffer configurations. I configured 2 transmit buffers. But the FLEXRAY_0.CH[1].MBIDXR.B.MBIDX field is still 0 even after setting an index. Do you know why is it so ?

Kind regards,

RSeba