cancel
Showing results for 
Search instead for 
Did you mean: 

Application configuration

szhan.7
Associate II

when i configure spc58nn project ,there is pineditor and clock tree ,the configurtion gui. and i cant find any other peripheral configuration gui,any one know this?

1 ACCEPTED SOLUTION

Accepted Solutions
ODOUV.1
ST Employee

select platform:0693W00000SwKFYQA3.pngthen click on +:0693W00000SwKFxQAN.pngthen select GTM:0693W00000SwKG7QAN.png

View solution in original post

11 REPLIES 11
ODOUV.1
ST Employee

Hello,

did you import an existing SPC58xNxx project ?

or did you created a new SPC58xNxx project ?

What would you need that you do not see ?

Best Regards.

ODOUV.1
ST Employee

Select the Platform component and click on the Green "+" to add others components (Init and LowLevelDrivers)

szhan.7
Associate II

0693W00000SwJlOQAV.png0693W00000SwJlnQAF.pngi import example project,there are only two items above,and i want to know if there is any other peripheral wizard,such as canfd ,SDADC or GTM and so on.

ODOUV.1
ST Employee

There are no other Graphical tools.

To configure SDADC or CAN, you need to add and configure the Low Level Drivers component:0693W00000SwK41QAF.pngFor GTM, you need to add and configure the GTM component:0693W00000SwK4LQAV.png 

You can take a look at GTM examples:0693W00000SwK4uQAF.png

0693W00000SwJlOQAV.png0693W00000SwJlnQAF.pngi import example project,there are only two items above,and i want to know if there is any other peripheral wizard,such as canfd ,SDADC or GTM and so on.

I can see low level Drivers component RLA,but i cant find GTM compennent==

ODOUV.1
ST Employee

select platform:0693W00000SwKFYQA3.pngthen click on +:0693W00000SwKFxQAN.pngthen select GTM:0693W00000SwKG7QAN.png

thank you very much :grinning_face:

you are welcome ;)