2022-09-26 08:14 PM
when i configure spc58nn project ,there is pineditor and clock tree ,the configurtion gui. and i cant find any other peripheral configuration gui,any one know this?
Solved! Go to Solution.
2022-09-27 01:00 AM
select platform:then click on +:
then select GTM:
2022-09-26 11:17 PM
Hello,
did you import an existing SPC58xNxx project ?
or did you created a new SPC58xNxx project ?
What would you need that you do not see ?
Best Regards.
2022-09-26 11:31 PM
Select the Platform component and click on the Green "+" to add others components (Init and LowLevelDrivers)
2022-09-26 11:35 PM
i import example project,there are only two items above,and i want to know if there is any other peripheral wizard,such as canfd ,SDADC or GTM and so on.
2022-09-27 12:29 AM
There are no other Graphical tools.
To configure SDADC or CAN, you need to add and configure the Low Level Drivers component:For GTM, you need to add and configure the GTM component:
You can take a look at GTM examples:
2022-09-27 12:29 AM
i import example project,there are only two items above,and i want to know if there is any other peripheral wizard,such as canfd ,SDADC or GTM and so on.
2022-09-27 12:52 AM
I can see low level Drivers component RLA,but i cant find GTM compennent==
2022-09-27 01:00 AM
select platform:then click on +:
then select GTM:
2022-09-27 01:12 AM
thank you very much :grinning_face:
2022-09-27 02:01 AM
you are welcome ;)