2025-01-09 9:38 PM
I am working on ism330dlc to find gyroscope x, y, and z values. I am getting x, y, and z values. I am also getting variable x, y, and z values when the board is maintained constant. I wrote registers are 0x1204,0x1160,0x1060,0X22,0X23,0X24,0X25,0X26, and 0X27. Pleas
Solved! Go to Solution.
2025-01-10 12:23 AM
Hi @Saikumar_avantel ,
Can you share a screenshot and the log file of the acquired data?
Thanks!
2025-01-10 12:23 AM
Hi @Saikumar_avantel ,
Can you share a screenshot and the log file of the acquired data?
Thanks!
2025-01-10 1:26 AM
I'm not using the controller. I'm using FPGA.
2025-01-10 1:29 AM
Ok, but can I see this variation in the output? Which is the order of magnitude?
2025-01-10 1:30 AM
The spi clock is 1MHz, and the delay between commands is 10 milliseconds. I don't have stored values, but if you want the source, I can share it.
2025-01-10 1:32 AM
what do mean about magnitude?
2025-01-13 1:15 AM
yes, it could be useful to understand the variation!
2025-01-15 9:12 PM
What do u mean magnitude ? isn't ODR ?
are please provide sequence list of registers to get GYRO data from ISM330dlc
2025-01-15 10:13 PM
if it is possible to offer technical support (such as Skype or Microsoft Teams). I'll show you my screen so you can help me figure out what's wrong.