cancel
Showing results for 
Search instead for 
Did you mean: 

Working on ISM330dlc

I am working on ism330dlc to find gyroscope x, y, and z values. I am getting x, y, and z values. I am also getting variable x, y, and z values when the board is maintained constant. I wrote registers are 0x1204,0x1160,0x1060,0X22,0X23,0X24,0X25,0X26, and 0X27. Pleas

1 ACCEPTED SOLUTION

Accepted Solutions
Federica Bossi
ST Employee

Hi @Saikumar_avantel ,

 

Can you share a screenshot and the log file of the acquired data?

Thanks!

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

5 REPLIES 5
Federica Bossi
ST Employee

Hi @Saikumar_avantel ,

 

Can you share a screenshot and the log file of the acquired data?

Thanks!

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

I'm not using the controller. I'm using FPGA.

Ok, but can I see this variation in the output? Which is the order of magnitude?

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

The spi clock is 1MHz, and the delay between commands is 10 milliseconds. I don't have stored values, but if you want the source, I can share it.

what do mean about magnitude?