cancel
Showing results for 
Search instead for 
Did you mean: 

With the help of iks01a3 sensors is it possible to detect the person is in sitting or in standing position

Gk.1
Associate II
 
1 REPLY 1
Eleon BORLINI
ST Employee

Hi @Gk.1​ ,

yes it is. You can refer -for example- to the MotionSD standing vs sitting desk detection library in the X-CUBE-MEMS1 firmware package that natively runs on the IKS01A3 platform: it provides real-time information about the user working mode (sitting at the desk or standing desk position), and is mostly intended for wrist-worn devices.

There is also the MotionAR activity recognition library that can be used for your application.

if this code is some help for your purpose, please select this answer as "best".

-Eleon