cancel
Showing results for 
Search instead for 
Did you mean: 

What is the vibration frequency range that the sensor can successfully detect?

ILARIASOFIA.GRASSI
ST Employee
1 ACCEPTED SOLUTION

Accepted Solutions
Denise SANFILIPPO
ST Employee

The output data rate of the sensor goes up to 6667 Hz, however the actual bandwidth of the sensor (-3dB point) is around 1.0 kHz.

View solution in original post

1 REPLY 1
Denise SANFILIPPO
ST Employee

The output data rate of the sensor goes up to 6667 Hz, however the actual bandwidth of the sensor (-3dB point) is around 1.0 kHz.