cancel
Showing results for 
Search instead for 
Did you mean: 

What is MP23ABS1TR start up time?

OPush
Associate II

What time is needed for MP23ABS1TR is ready after power On?

(The idea is to decrease MP23ABS1TR current consuption by power strobing)

BR, Oleg

1 REPLY 1
Eleon BORLINI
ST Employee

Hi @OPush​ , the MP23ABS1TR dataout is ready (i.e. the sensitivity falls inside +-1dB guardband with respect to the long-term settled value) after less then 10ms from the power up event. You can decrease the current consumption lowering the Vdd value, but i suggest you to stay above 2V in order not to decrease the overall THD performances. Regards