2019-07-08 7:22 PM
I am using STEVAL-MKSBOX1V1 and I want to do some changes in the firmware.
What in-circuit debugger/programmer should I use? Should I use ST-LINK/V2 or STLINK-V3SET or STLINK-V3MINI?
Please help me. Thank you
Solved! Go to Solution.
2019-07-31 7:11 AM
Because you cannot plug a 20 pin cable on the SensorTile.box... Pls note that you could have the 5x2 header instead of the 7x2 header on your sensortile.box... could you please send me a picture of it? Regards
2019-07-31 7:31 AM
Sorry I forgot that it is only a 14 pins. I cannot send the picture right now because the SensorTile.Box is in our office and I am at home right now. I will send it tomorrow (GMT +8). By the way I have a flat ribbon connector that is included in the STLINK-V3 that I bought, can I use the flat ribbon connector that is STDC14 output to ARM20-compatible connector?
2019-08-01 3:08 AM
uhm.. I don't think the ribbon cables are compatible for this purpose... I suggest you to directly connect the VDD, GND, SWDIO and SWCLK with bridges... Regards
2019-08-01 6:49 PM
Ok I understand. I will try it as soon as I receive the STLINK-V2. Thank you
2019-08-02 4:52 AM
Please note for the sake of completeness that you can now find the Sensortile.box schematic online. Regards
2019-08-05 1:36 AM
Hi @Eleon BORLINI with regards to the SensorTile.box connection to the STLINK-V2, I just want to clarify what pins from SensorTile.box do I need to connect to STLINK-V@?
Am I right that it is pin no: 3, 4, 5, 6 ? or pin no: 3, 4, 5, 6, 13, 14?
Thank you
2020-04-13 10:20 AM
Anything new about adapter board with dedicated level shifters and LDOs for the 1.8V debugging?
In UM2448 chapter 12 B-STLINK-VOLT board extension description shows this but actual board is still missing.
2020-04-14 5:47 AM
Hi @savimakt , good question... I added the ST-LINK Utility and the STLINK-V3 topics to the original question for eventual support. Regards