I am using STEVAL-MKSBOX1V1 and I want to do some changes in the firmware. What in-circuit debugger/programmer should I use? Should I use ST-LINK/V2 or STLINK-V3SET or STLINK-V3MINI?Please help me. Thank you
Hi @Eleon BORLINI with regards to the SensorTile.box connection to the STLINK-V2, I just want to clarify what pins from SensorTile.box do I need to connect to STLINK-V@? Am I right that it is pin no: 3, 4, 5, 6 ? or pin no: 3, 4, 5, 6, 13, 14?Thank ...
Sorry I forgot that it is only a 14 pins. I cannot send the picture right now because the SensorTile.Box is in our office and I am at home right now. I will send it tomorrow (GMT +8). By the way I have a flat ribbon connector that is included in the ...
Hi @Eleon BORLINI Ok I understand. The STLINK-V2 package includes also a JTAG or SWD and SWV flat ribbon with a 20-pin connector but you are telling me that I should use 7x2-to-5x2 adapter. SensorTile.Box have a JTAG on the PCB, so can I use the JTA...