2022-11-02 07:21 AM
2022-11-03 08:20 AM
Hello ,
Yes for both.
In the meantime, I have installed the following : VCP_V1.5.0_Setup_W8_x64_64bits.exe and it works now.
But, normally I should not have done this according to STm video "Getting started with profiMEMS" explaining needed driver are already native in the files.zip
2022-11-03 08:08 AM
Hi @LCari.1 ,
can you see the STM32 board in the device manager?
And did you uploaded the last firmware update on the STEVAL-MKI109V3?
-Eleon
2022-11-03 08:20 AM
Hello ,
Yes for both.
In the meantime, I have installed the following : VCP_V1.5.0_Setup_W8_x64_64bits.exe and it works now.
But, normally I should not have done this according to STm video "Getting started with profiMEMS" explaining needed driver are already native in the files.zip
2022-11-03 08:21 AM
Those are the win8 drivers, the win10 has already embedded the STM32 drivers... or at least it should
-Eleon
2022-11-03 08:25 AM
Yes that 's what I understood as well. no need for W10
BUT, it didn't work , the port was enumeraed in Device Manager but no way to communicate....
2022-11-03 08:27 AM
By the way, I have posted another issue on the web case 00167097:
I have downloaded the UNICO GUI software to develop an apps using the accelerometer ref = LIS2DW12 with the STEVAL-MKI109V3 (Professional MEMS tool).
When clicking on the <Advanced Features> in option tab , the "current supply measurement / power supply" window does not pop up. No way to measure the current which is the basics.... Moreover, it enters in an never ending loop with UNICO is not responding !
Could you help on that one ?
Thanks
2022-11-03 08:43 AM
coming back to FW version: I have V2.18.6 coming with download of GUI UNICO V9.13.0.0.
Is it correct?
In the UM1049 I read 3.30.0
2022-11-03 09:07 AM
Hi @LCari.1 ,
the associated Unico FW should be the v 3.42.4 version
-Eleon
2022-11-03 09:12 AM
Yes , I have the V3.42.4
2022-11-03 09:15 AM
The interface has many less tabs and options than the on described in the UM1049