Skip to main content
kaygee
Associate II
Oct 10, 2022 5:57 AM UTC
Solved

How do you calculate LSM6DS3TR-C X,Y and Z user offsets?

Is there simple and straight-forward way to calculate the user offsets and store it in the relevant register

    This topic has been closed for replies.
    Eleon BORLINI
    Eleon BORLINIBest answer
    ST Employee
    Oct 10, 2022 2:15 PM UTC

    Hi @kaygee​ ,

    My suggestion is to characterize the LSM6DS3 offset in a known position, typically perfectly flat on a floor, with the z axis pointing upwards. Then you can store the found value in the user registers and it will be automatically applied to the data-out stream.

    -Eleon

    5 replies

    Eleon BORLINI
    Eleon BORLINIBest answer
    ST Employee
    Oct 10, 2022 2:15 PM UTC

    Hi @kaygee​ ,

    My suggestion is to characterize the LSM6DS3 offset in a known position, typically perfectly flat on a floor, with the z axis pointing upwards. Then you can store the found value in the user registers and it will be automatically applied to the data-out stream.

    -Eleon

    kaygee
    kaygeeAuthor
    Associate II
    Oct 11, 2022 2:08 PM UTC

    Hi @Eleon BORLINI​ 

    Noted, Thanks

    kaygee
    kaygeeAuthor
    Associate II
    Nov 4, 2022 1:52 PM UTC

    @Eleon BORLINI

    I have a Adafruit breakout board of the LSM6DS3TR-C.

    I managed to I2C communication working between the PIC-microcontroller and the LSM6DS3TR-C.

    I am able to read the XYZ register for the Accelerometer, the Gyroscope and the Magnometer.

    The problem is I tried to get data fused so I can compute the Pitch, Roll and Yaw. My problem is my values jump around and they are not consistent. Since I could not find an example of how to compute the Pitch, Roll and Yaw values. I based my program on the code written by Kris Winer for the LSM9DS1 (https://github.com/kriswiner/LSM9DS1/blob/master/LSM9DS1_BasicAHRS_Nano33.ino), Because I could not find the appropriate code for the LSM6DS3TR-C. I had a look at the code suggested by ST, on Github (https://github.com/STMicroelectronics/lsm6ds3tr-c-pid) which I found to be too basic for what I am trying to do. There is nothing about fusing data after reading it.

    As you suggested that I lay the breakout board flat on a table and take a few measurements. Then store them in the user offset registers. The problem is I do not understand how the below fits into calculating the offsets.

    CTRL6_C register description

    USR_OFF_W: Weight of XL user offset bits of registers X_OFS_USR (73h),

    FUNC_CFG_ACCESS (01h), Z_OFS_USR (75h)

    0 = 2-10 g/LSB

    1 = 2-6 g/LSB

    So I made the user offsets all zeros

    X_OFS_USR (73h) = 0,

    X_OFS_USR (74h) = 0,

    Z_OFS_USR (75h) = 0,

    And still the Pitch, Roll and Yaw values still jump around a lot.

    Is there any website or example code you can point me to, which I can use as an example for my application

    kaygee
    kaygeeAuthor
    Associate II
    Nov 4, 2022 2:15 PM UTC

    The typical offset values calculated are:

    Offset_X = 105

    Offset_Y = -1353

    Offset_Z = 17573

    The question is how do I store these values in the 8 bit user offset registers

    kaygee
    kaygeeAuthor
    Associate II
    Nov 4, 2022 2:30 PM UTC

    The code from Adafruit is unnecessarily bloated because they try to cater for a lot of accelerometers in one program