cancel
Showing results for 
Search instead for 
Did you mean: 

STEVAL-PROTEUS: Serial Monitor over Micro USB

Haze
Associate

Hi all!

I've recently started working on a fault classification model utilizing the proteus1 board and the NEAI studio suite. I'd ideally like to set up a serial datalogger via the onboard micro USB to both obtain and display readings, alongside benchmarking models. Connecting the proteus with the datalogger flashed via FUOTA (As I don't have a STLINK V3MINIE on hand) leads to it not being recognized when trying to select a COM port to obtain readings. I'd be grateful if anyone would be kind enough to tell me if I'm missing anything, or if there are specific COM drivers for this.

 

Thanks in advance

1 REPLY 1
Federica Bossi
ST Employee

Hi @Haze ,

Did you install the STSW-PROTEUS1 v1.1.1. via FUOTA? If yes, then you need to power off the board before using it.

In addition, I suggest using the BLE stack version 1.20.0 from Github project STM32CubeWB.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.