cancel
Showing results for 
Search instead for 
Did you mean: 

STEAL-STWINKT1 live data reading

bcryhun
Associate II

Hello everyone,

i have STEAL-STWINKT1 board. It has some sensor on it. I want to see these data live on screen and save these values. I dont need to plot fft. How can i do that without using coding with hal libraries.

 

Thank you

2 REPLIES 2
SimonePradolini
ST Employee

Hi @bcryhun 

ST offers ready-to-use code examples. You are free to download and modify for your purposes.

Have a look at FP-SNS-DATALOG1 of FP-IND-PREDMNT1; those examples could fit your request.

We are also working to include STWIN in FP-SNS-DATALOG2, an extended version of the above-mentioned FP-SNS-DATALOG1.

Best regards

Simone

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
AScha.3
Chief III

How can i do that without using coding with hal libraries.

no problem. read RM and write to registers... bare metal  . called. up to you , ymmv .

If you feel a post has answered your question, please click "Accept as Solution".