ST LIS2DE12 WHO_AM_I?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-01-08 9:58 PM
Dear ST Community Members,
I tried to understand...page 25 ST LISDE12.pdf
..................
Data are transmitted in byte format (DATA). Each data transfer contains 8 bits. The number
of bytes transferred per transfer is unlimited. Data is transferred with the Most Significant bit
(MSb) first. If a receiver can’t receive another complete byte of data until it has performed
some other function, it can hold the clock line, SCL low to force the transmitter into a wait
state. Data transfer only continues when the receiver is ready for another byte and releases
the data line. If a slave receiver doesn’t acknowledge the slave address (i.e. it is not able to
receive because it is performing some real-time function) the data line must be left HIGH by
the slave. The master can then abort the transfer. A low-to-high transition on the SDA line
while the SCL line is HIGH is defined as a STOP condition. Each data transfer must be
terminated by the generation of a STOP (SP) condition.
In order to read multiple bytes, it is necessary to assert the most significant bit of the subaddress
field. In other words, SUB(7) must be equal to 1 while SUB(6-0) represents the
address of the first register to be read.
In the presented communication format MAK is Master acknowledge and NMAK is No
Master Acknowledge.
........................
Table 16 to Table 19....
How can I generate SAK and SUB ?
Here's the code I have made :
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_4, GPIO_PIN_SET); //ACC_CS =1 I2C MODE
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_5, GPIO_PIN_RESET); //ACC_A0 =0 SA0=0
HAL_Delay(100);
//WHO_AM_I, read ,register address 0F 000 1111, 00110011 = 33h page 30 ST LIS2DE12
buffer[0] = 0x0F;
HAL_I2C_Master_Transmit(&hi2c1, 0x31>>1 ,buffer ,1, 100); //transmit one byte to ST LIS2DE12
//HAL_StatusTypeDef HAL_I2C_Master_Transmit(I2C_HandleTypeDef *hi2c, uint16_t DevAddress, uint8_t *pData, uint16_t Size, uint32_t Timeout)
// put HAL_I2C_Receive after this give a delay 10ms, how many bytes do I want to read from the register.
HAL_Delay(10);
HAL_I2C_Master_Receive(&hi2c1, 0x31>>1 ,buffer ,2, 100); //receive one byte to ST LIS2DE12
//HAL_StatusTypeDef HAL_I2C_Master_Receive(I2C_HandleTypeDef *hi2c, uint16_t DevAddress, uint8_t *pData, uint16_t Size, uint32_t Timeout)
rawValue = buffer[0]<<8 | buffer[1];
//buffer[0] -- MSB
//buffer[1] -- LSB
printf("This is from ST LIS2DE12 : %s",rawValue);
//printf("\r\n");
//printf("%s",result);
HAL_Delay(1000);
Any clues ?
Thanks
- Labels:
-
Accelerometers
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-01-09 12:51 AM
I follow
ST ==> SAD+W ==> SAK ==> SUB ==> SAK ==> SR ==> SAD+R ==> SAK ==> DATA ==> NMAK ==> SP ----------------> Reading 1 byte from ST LIS2DE12
from Table 18
page 25 ST LIS2DE12 datasheet....
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-01-09 1:12 AM
Subaddress byte (SUB) is automaticaly generated by HAL_I2C_Master_Transmit or HAL_I2C_Master_Receive.
Slave acknowledge (SAK) is generated by the sensor (I2C slave).
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-01-14 6:18 PM
Thanks for the answer Miroslav,
If I want to make the sensor very sensitive to movement,
which register do we need to change ?
I saw INT2_THS (36h), and INT1_THS (32h), any other registers that I need to change to make it more sensitive ?
Thanks