2024-08-20 06:01 AM
Hello all,
I wanted to use sensortile to collect data on microsd card. (I have two of them)
So, One portable cradle from the kit working good, but another is not working with the same microsd card.
When start it from the android app the sensor just behave like normal but after several seconds disable sd logging completely. Need to say that I do not see any files on SD card after the procedure.
Also, I did check solder joints and didn't notice any problems with soldering.