2021-04-16 04:11 AM
Hi,
Am trying to connect SensorTile Box Using St-Link to flash the Program. But When I connect in DFU mode "USB" is getting detected, but through ST-Link V2, the serial numbers getting detected but am not able to connect. It says "STM32 Target not found".
I have attached 2 images for ref. Please confirm which connections are correct.
Image 1- I have connected the St-Link with Jtag in the Adapter.
Image 2- I have attached the adapter directly into the St-Link.
Also Please clarify "How to Connect the ST-LInk V2 in DFU mode in CubeProgrammer?".
Regards,
Shivashankari.
Solved! Go to Solution.
2021-05-03 08:39 AM
Hi, two screens shots to be shared for an IDE setup and CubeProg. Please check.
2021-04-19 01:31 AM
Hi @ShivaRagu ,
did you already check this post, that explains how to upload .bin file on SensorTile.box in DFU mode?
You can also refer to the attached video, that focuses on the use of STM32CubeProgrammer for the tool.
Please check if you have performed all the steps in these tutorials, especially if you set the Full Chip Erase flag.
-Eleon
2021-05-03 08:39 AM
Hi, two screens shots to be shared for an IDE setup and CubeProg. Please check.