cancel
Showing results for 
Search instead for 
Did you mean: 

Problems to pair SensorTile.box to ST BLESensor Application. Basically it scans for nearby boards and then gives an error loading the App. What can I do?

ATrif.1
Associate II

0693W00000Hr62RQAR.jpg

7 REPLIES 7
Eleon BORLINI
ST Employee

HI @ATrif.1​ ,

which application are you trying to upload on your SensorTile.box? An already-built one (Mode1) or a custom one (Mode2)?

I see that the, so you correctly paired the devices, right (using the 123456 code)?

-Eleon

ATrif.1
Associate II

Hi Eleon,

Basically I follow this pathway : Create an application - Vibration Monitor - Vibration Monitor compare.

And the first time SensorTile.box was connected to the mobile App i used 123456 code to pair it.

Hi @ATrif.1​ ,

It might be related to the Vibration Monitor compare only. Are you facing the issue also while uploading other predefined apps?

The "Vibration Monitor compare" needs a csv file on the SD card, which is the reference for the vibration monitor comparison. You can create it in a first step, writing an acceleration pattern on the SD card, and then try again uploading the Vibration Monitor compare app.

-Eleon

Hi Eleon,

Well, I also tried to upload other predefined apps, but unfortunately this problem persists.

Hi @ATrif.1​ ,

does the problem persist with all the predefined apps or only with some ones?

-Eleon

Hi @Eleon BORLINI​ 

The problem persists with all predefined apps, can the problem be with Bluetooth protocol?

Hi @ATrif.1​ ,

it might be... you might try to restore the Sensortile.box firmware to the factory one in the way described in this post (LINK), but not sure this can be the solution.

-Eleon