2022-01-10 04:53 AM
2022-01-12 06:09 AM
HI @ATrif.1 ,
which application are you trying to upload on your SensorTile.box? An already-built one (Mode1) or a custom one (Mode2)?
I see that the, so you correctly paired the devices, right (using the 123456 code)?
-Eleon
2022-01-13 07:08 PM
Hi Eleon,
Basically I follow this pathway : Create an application - Vibration Monitor - Vibration Monitor compare.
And the first time SensorTile.box was connected to the mobile App i used 123456 code to pair it.
2022-01-14 03:19 AM
Hi @ATrif.1 ,
It might be related to the Vibration Monitor compare only. Are you facing the issue also while uploading other predefined apps?
The "Vibration Monitor compare" needs a csv file on the SD card, which is the reference for the vibration monitor comparison. You can create it in a first step, writing an acceleration pattern on the SD card, and then try again uploading the Vibration Monitor compare app.
-Eleon
2022-01-18 04:55 PM
Hi Eleon,
Well, I also tried to upload other predefined apps, but unfortunately this problem persists.
2022-01-21 02:27 AM
Hi @ATrif.1 ,
does the problem persist with all the predefined apps or only with some ones?
-Eleon
2022-05-05 05:41 AM
Hi @Eleon BORLINI
The problem persists with all predefined apps, can the problem be with Bluetooth protocol?
2022-05-09 02:58 AM
Hi @ATrif.1 ,
it might be... you might try to restore the Sensortile.box firmware to the factory one in the way described in this post (LINK), but not sure this can be the solution.
-Eleon