cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with setup of HS sensor DataLog application for STWINKT1

RMess.1
Associate

Hello everyone, i'm a beginner,

I recently bought a STWINKT1. I'm trying to setup the HSDataLog, using the: '' quick start guide HS sensor dataLog application for STWINKT1. Running USB_DataLog_Run.bat the results is: no devices. I installed STM32CubeProgrammer, and the software correctly work. Do you have any suggestions?

Thanks

2 REPLIES 2
Eleon BORLINI
ST Employee

Hi @RMess.1​ , sorry for the late feedback mostly due to vacation time... if I well understand your problem, you run USB_DataLog_Run.bat but it is not able to detect you, right? Did you configured the related VCOM port in the correct way (as shown in the below picture)?

0693W000002lWpDQAU.png

I also suggest you to give a look at this article, which may help you to deal with the Example – HS_DataLog --> http://www.emcu.eu/mems-predictive-maintenance-using-an-intelligent-logging-kit-for-iot-applications/

Regards

Eleon BORLINI
ST Employee

Hi @RMess.1​ ,

please check this other thread if it can be of some help.

-Eleon