2024-01-31 12:40 AM
At this point, the I2C statuses all look normal. I have written code to extract temperature and humidity data values via high-resolution single-shot mode, but the data values are not being extracted correctly. Do I need to set the high-speed mode and access write, read before entering single-shot mode? I don't know what the heck is wrong.
board:NUCLEOF303K8 / sensor: SHT30DLS, gpio / i2c source and header file is no problem / i2c = fast mode
if you help me. i'm will bless to you every every every day...
Solved! Go to Solution.
2024-01-31 5:41 AM
Second reply
in your conv you
calc *Temperature = -40.0f + 125.0f * ((float)tempRaw / 65535.0f);
in the datasheet it is
so there is a wrong formular in your source code.
padawan
2024-01-31 5:16 AM
Ok some questions:
why do you not use the HAL_I2C_Master_Transmit ans HAL_I2C_Master_Receive?
There are some "Pullups" on SDL SCL?
The first command to the Sht3xx i send is "WriteCommand(CMD_MEAS_POLLING_H);"
By
uint8_t sht3x::WriteCommand(etCommands command)
{
etError error; // error code
HAL_StatusTypeDef _hal;
uint8_t _sbuff[2] ={0x00, 0x00}; // Array to transmit /PE
_sbuff[0] = (command >> 8);
_sbuff[1] = (command & 0xFF);
_hal = HAL_I2C_Master_Transmit(_i2c,_adr, _sbuff, 2,1000);
_ok = _hal;
error = (etError)_ok;
return error;
}
If you read from the Sensor you have to read 3 Bytes, 2 data and CRC
or 5 bytes (2 Temp 2 Hum 1 CRC).
If you look at https://www.sensirion.com/products/downloads/?category=Humidity
in section Software Sample Code SHT3x.
I change the "i2c.h" and "i2c.c" to the STM HAL.
You can first read the serialnumber before you try to read and calculate the temp.
HTH
padawan
2024-01-31 5:41 AM
Second reply
in your conv you
calc *Temperature = -40.0f + 125.0f * ((float)tempRaw / 65535.0f);
in the datasheet it is
so there is a wrong formular in your source code.
padawan
2024-01-31 11:04 PM
Thank you for your response. I apologize for the delay in getting back to you.
The code I'm currently writing is intended to be written entirely in C, to build a foundation and avoid using the HAL library as much as possible. I changed the formula, thanks a lot!!!! :)