cancel
Showing results for 
Search instead for 
Did you mean: 

LSM9DS1 magnetometer interrupts - open-drain or push/pull?

Bill Burgess
Associate II
Posted on May 08, 2017 at 01:17

The LSM9DS1 data sheet shows that the accelerometer/gyroscope module's two interrupts can be configured either as open-drain or push/pull.  However, I am missing the description of the magnetometer module's interrupt.  I assume that means it is fixed and cannot be user-configured.  Is it fixed as open-drain type, or as push/pull type?

#interrupts #lsm9ds1 #push-pull-output-or-open-drain-output
1 ACCEPTED SOLUTION

Accepted Solutions
Posted on May 19, 2017 at 16:06

The INT_M interrupt pin is also push-pull.

View solution in original post

3 REPLIES 3
Miroslav BATEK
ST Employee
Posted on May 10, 2017 at 15:52

The DRDY_M (Magnetic sensor data ready) pin is push-pull, with active high level.

Posted on May 10, 2017 at 20:12

Thanks, that helps.  But I was actually asking about the magnetometer interrupt, Pin 10, INT_M.  I couldn't find anything in the data sheet saying whether it's push-pull or open drain.  The active level (high/low) can be configured in software but not, apparently, the output type.  Do you know which it is?

Posted on May 19, 2017 at 16:06

The INT_M interrupt pin is also push-pull.