2020-11-04 6:04 AM
Hi Team,
I am trying to add support for magnetometer LIS3MDL module using the following linux driver https://github.com/STMicroelectronics/STMems_Linux_IIO_drivers/tree/linux-4.9.y-gh/drivers/iio/magnetometer. If I add interrupt in device tree the module is not registering the iio device.
lis3mdl@1c {
compatible = "st,lis3mdl";
reg = <0x1c>;
interrupt-parent = <&gpio>;
interrupts = <65 IRQ_TYPE_LEVEL_HIGH>;
vdd-supply = <&p3449_vdd_1v8>;
vddio-supply = <&p3449_vdd_1v8>;
};
I got the folloiwng error.
[ 5.150951] iio iio:device10: interrupts active high level
[ 5.198445] iio iio:device10: failed to request trigger IRQ.
If I remove the interrupt from the devicetree the device is getting registered but I am not able to use interrupt. Is there any other way to use interrupt in magnetometer ?
Can you please help me to solve this issue,
Regards,
Ajith.
2020-11-09 6:07 AM
Hi Ajith @AKuma.12esh ,
Are you referring to the magnetometer interrupts, such as the ones described in the application note AN5069 p.21 (it's for LIS2MDSL ok, but just for understand)
If so, I believe you should define the register and the write function, for example in the st_mag3d_core.c file.
#define ST_MAG3D_INT_CFG_ADDR 0x0f
#define ST_MAG3D_INT_CFG_VAL 0xe7and then define the appropriate function based on:
static int st_mag3d_write_with_mask(struct st_mag3d_hw *hw, u8 addr,
u8 mask, u8 val)Then you have to check the INT pin with your application processor.
-Eleon