cancel
Showing results for 
Search instead for 
Did you mean: 

LSM9DS1 - how should I understand the fields of the CTRL_REG2_G (0x11) register

kobelev
Associate

The datasheet on the LSM9DS1 chip on page 47 is very unclear on how the configuration of filters is supposed to work. They just tell that the fields INT_SEL and OUT_SEL are existing and give this diagram:

0693W00000SvxhZQAR.png 

I have hard time trying to understand what those dashed lines might mean. Why are they dashed? I understand that INT_SEL and OUT_SEL are similar. So, I give just one table below. I tend to decipher the situation this way:

0693W00000SvxkAQAR.pngCan anybody comment if my guess is right and what should I put into the missing fields?

1 ACCEPTED SOLUTION

Accepted Solutions
kobelev
Associate

So, I would rewrite the picture above (just the data channel since the interrupts channel is similar) this way:

0693W00000Un9lOQAR.pngThe same in the table form:

0693W00000Un9lTQAR.png 

View solution in original post

2 REPLIES 2
Eleon BORLINI
ST Employee

Hi @kobelev​ ,

The table is ok, and when OUT_SEL == 01 is selected, if the HP_EN == 0 (CTRL_REG3_G (12h)), then the acquired signal will only pass through LPF1, while if HP_EN == 1 the resulting chain would be LPF1 + HPF.

-Eleon

kobelev
Associate

So, I would rewrite the picture above (just the data channel since the interrupts channel is similar) this way:

0693W00000Un9lOQAR.pngThe same in the table form:

0693W00000Un9lTQAR.png