cancel
Showing results for 
Search instead for 
Did you mean: 

IIS3DWB FIFO readout wrap-around

LKert
Associate

Hi
does the wrap-around feature work for the FIFO output registers as well?
Can I just enable wrap-around in CTRL5 register, and read 7*number of words in FIFO bytes starting with register 78h to get the entire content of the FIFO?

I have a hard time retrieving the data in time, Tiva C lib takes way too long to start and stop SPI transactions. Now I don't have the hw with me to simply test it.

thanks,
Lorand

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Federica Bossi
ST Employee

Hi @LKert ,

As described in the Application Note, the wrap around is automatically done when you are using the FIFO: you will read the 9 output registers:

FedericaBossi_0-1700218302243.png

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.