2024-05-16 03:39 AM
Hi
I was looking at how a register read works for LSM6DSL
https://www.st.com/en/embedded-software/stsw-fcu001.html
I found the function below. Does the number/amount of __asm("dsb\n") correspond to SPI clk?
Is there no easier way to do this? Like using HAL_SPI_TransmitReceive(...)?
/**
* @brief This function reads a single byte on SPI 3-wire.
* @param xSpiHandle : SPI Handler.
* @param val : value.
* @retval None
*/
void SPI_Read(SPI_HandleTypeDef* xSpiHandle, uint8_t *val)
{
/* In master RX mode the clock is automaticaly generated on the SPI enable.
So to guarantee the clock generation for only one data, the clock must be
disabled after the first bit and before the latest bit */
/* Interrupts should be disabled during this operation */
__disable_irq();
//GPIOA->BSRR = (uint32_t)GPIO_PIN_8 << 16U;
__HAL_SPI_ENABLE(xSpiHandle);
__asm("dsb\n");__asm("dsb\n");
__asm("dsb\n");__asm("dsb\n");
__asm("dsb\n");__asm("dsb\n");
__asm("dsb\n");__asm("dsb\n");
__asm("dsb\n");__asm("dsb\n");
__asm("dsb\n");__asm("dsb\n");
__asm("dsb\n");__asm("dsb\n");
__asm("dsb\n");__asm("dsb\n");
__asm("dsb\n");__asm("dsb\n");
__asm("dsb\n");__asm("dsb\n");
__asm("dsb\n");__asm("dsb\n");
__asm("dsb\n");__asm("dsb\n");
__asm("dsb\n");__asm("dsb\n");
__asm("dsb\n");__asm("dsb\n");
__asm("dsb\n");__asm("dsb\n");
__asm("dsb\n");__asm("dsb\n");
__asm("dsb\n");__asm("dsb\n");
__asm("dsb\n");__asm("dsb\n");
__asm("dsb\n");__asm("dsb\n");
__asm("dsb\n");__asm("dsb\n");
__asm("dsb\n");__asm("dsb\n");
__asm("dsb\n");__asm("dsb\n");
__asm("dsb\n");__asm("dsb\n");
__asm("dsb\n");__asm("dsb\n");
__asm("dsb\n");__asm("dsb\n");
__asm("dsb\n");__asm("dsb\n");
__asm("dsb\n");__asm("dsb\n");
__asm("dsb\n");__asm("dsb\n");
__asm("dsb\n");__asm("dsb\n");
__asm("dsb\n");
__asm("dsb\n");
__asm("dsb\n");
__asm("dsb\n");
__asm("dsb\n");
__asm("dsb\n");
__asm("dsb\n");
__asm("dsb\n");
__asm("dsb\n");
__HAL_SPI_DISABLE(xSpiHandle);
__enable_irq();
while ((xSpiHandle->Instance->SR & SPI_FLAG_RXNE) != SPI_FLAG_RXNE);
/* read the received data */
*val = *(__IO uint8_t *) &xSpiHandle->Instance->DR;
while ((xSpiHandle->Instance->SR & SPI_FLAG_BSY) == SPI_FLAG_BSY);
}
2024-07-09 01:59 AM
Hi @MK..1 ,
The software example that you share was a first release, it works but it is open to improvements.
__asm("dsb\n") function in the example is used to introduce delay and synchronize communication.
I suggest to test the communication with the function provided in the example and then test the code substituting it with HAL.