2018-11-05 7:19 AM
Hi,
I am using the setup with LSM6DSL + LIS2MDL. All works fine, with the exception that once started the conversion to FIFO with sensor fusion, at 104 sps, I observe significant periodical (around 22 samples cycles) noise on the last acceleration axis (Z). With LIS2MDL stopped there is no noise. More, if I disable the internal pull-up resistors, the noise disappears as well.
Any advice on this?
Many thanks,
Florin
Solved! Go to Solution.
2018-11-06 4:46 AM
Good to hear.
Indeed, the datasheet is not very clear.
You can also refer to application note AN5040 which goes more into details.
2018-11-05 7:36 AM
First can you share your schematic?
2018-11-05 8:42 AM
2018-11-06 1:07 AM
The schematic looks ok, but I have a few more questions:
2018-11-06 4:33 AM
Hi Miroslav,
Thank you for your time, and valuable questions!
The answers are as follows:
"START_CONFIG
Sensor Hub trigger signal selection. Default value: 0
(0: Sensor hub signal is the XL/Gyro data-ready;
1: Sensor hub signal external from INT2 pad.)"
After configuring it as per your suggestion (OK, done at the right time in the initialization sequence of the assembly), all works like a charm!
Thank you!
Florin
2018-11-06 4:46 AM
Good to hear.
Indeed, the datasheet is not very clear.
You can also refer to application note AN5040 which goes more into details.
2018-11-06 4:52 AM
Thank you Miroslav, indeed, the Application note is more clear, but all is easy after sorting it out :beaming_face_with_smiling_eyes:.
2024-04-04 10:53 PM
Hi can u please explain me how did u connect lsm6dsl and lis2mdl and what are the things u configured. Like how did u know what to configure. Also one last thing how did u plot.