2020-02-18 06:10 PM
Hi,
As stated in question, accelerometer vector magnitudes are different when sensors are oriented to +X axis and - X axis. Difference is about 5 %.
DT0105 only states about +X axis calibration. so I'm confused whether this difference comes from chip itself, or installation.
Solved! Go to Solution.
2020-02-19 01:32 AM
Hi @MKang.1 , are you measuring data at application level? If so, did you check if you are fully planar with respect to x-direction (board / soldered device / etc), in order to avoid an "environmental" offset. Supposing it is an offset of any type, it is possible to compensate an unwanted offset in two different ways:
Regards,
Eleon
2020-02-19 01:32 AM
Hi @MKang.1 , are you measuring data at application level? If so, did you check if you are fully planar with respect to x-direction (board / soldered device / etc), in order to avoid an "environmental" offset. Supposing it is an offset of any type, it is possible to compensate an unwanted offset in two different ways:
Regards,
Eleon
2020-02-19 01:41 AM
Hi Eleon,
I understood I need to calibrate an offset. To calculate offset value, can I refer to DT0053 also for LSM6DSL?
Thanks for prompt answer.
Regards,
Kang
2020-02-19 01:48 AM
Yes, the mentioned design tips are generic and can be used also for LSM6DSL.
You can refer also to this community topic.
Regards
2020-02-19 01:53 AM
Now it seems clear. Thanks!