2019-08-27 4:15 AM
Hi,
I'm trying to configure the AWT function in the LSM6DSL. All works fine minus the latency. I change the latency to 0x01(40ms) but the interrupts keep with a delay of 600ms(default) between each one. Any idea what I'm doing wrong?
Accelerometer band width : 100Hz
Accelerometer range : 2g
Accelerometer sample rate : 26Hz
Gyro Disabled
Configuration Reference: https://www.st.com/content/ccc/resource/technical/document/application_note/group0/26/07/3f/bf/12/55/47/62/DM00402563/files/DM00402563.pdf/jcr:content/translations/en.DM00402563.pdf - page 56
Configuration code:
// Enable access to embedded registers (bank B)
// Write A0h to FUNC_CFG_ACCESS
ret = writeRegister(LSM6DSL_ACC_GYRO_FUNC_CFG_ACCESS, LSM6DS3_ACC_GYRO_FUNC_CFG_ENABLED_B);
if (ret != IMU_SUCCESS)
return ret;
// Set latency
ret = writeRegister(LSM6DS3_ACC_GYRO_A_WRIST_TILT_LAT, lat);
if (ret != IMU_SUCCESS)
return ret;
// Set threshold
ret = writeRegister(LSM6DS3_ACC_GYRO_A_WRIST_TILT_THS, ths);
if (ret != IMU_SUCCESS)
return ret;
// Set mask
ret = writeRegister(LSM6DS3_ACC_GYRO_A_WRIST_TILT_MASK, mask);
if (ret != IMU_SUCCESS)
return ret;
// Disable access to embedded registers (bank B)
ret = writeRegister(LSM6DSL_ACC_GYRO_FUNC_CFG_ACCESS, LSM6DS3_ACC_GYRO_FUNC_CFG_DISABLED);
if (ret != IMU_SUCCESS)
return ret;
// Enable embedded functions
// Enable AWT detection
// Write 84h to CTRL10_C
//writeRegister(LSM6DS3_ACC_GYRO_CTRL10_C, LSM6DS3_ACC_GYRO_WRIST_TILT_EN_ENABLED);
ret = writeRegister(LSM6DS3_ACC_GYRO_CTRL10_C, 0x84);
if (ret != IMU_SUCCESS)
return ret;
// AWT interrupt driven to the INT2 pin
// Write 01h to DRDY_PULSE_CFG
ret = writeRegister(LSM6DS3_ACC_GYRO_DRDY_PULSE_CFG, 0x01);
if (ret != IMU_SUCCESS)
return ret;
// Enable latched mode
readRegister(LSM6DS3_ACC_GYRO_TAP_CFG1, &buf);
if (ret != IMU_SUCCESS)
return ret;
ret = writeRegister(LSM6DS3_ACC_GYRO_TAP_CFG1, (buf | LSM6DS3_ACC_GYRO_LIR_ENABLED));
#define LSM6DSL_ACC_GYRO_FUNC_CFG_ACCESS 0x01
#define LSM6DS3_ACC_GYRO_DRDY_PULSE_CFG 0x0B
#define LSM6DS3_ACC_GYRO_CTRL10_C 0x19
#define LSM6DS3_ACC_GYRO_TAP_CFG1 0x58
/**** Embedded functions register mapping - Bank B *******/
#define LSM6DS3_ACC_GYRO_A_WRIST_TILT_LAT 0x50
#define LSM6DS3_ACC_GYRO_A_WRIST_TILT_THS 0x54
#define LSM6DS3_ACC_GYRO_A_WRIST_TILT_MASK 0x59
#define LSM6DS3_ACC_GYRO_FUNC_CFG_ENABLED_B 0xA0
#define LSM6DS3_ACC_GYRO_FUNC_CFG_DISABLED 0x00
#define LSM6DS3_ACC_GYRO_LIR_ENABLED 0x01
Best regards.
Solved! Go to Solution.
2019-08-29 6:01 AM
Hi,
Found the problem. The problem was that the pin of the INT2 in the MCU have debounce timeout.
Best regards.
2019-08-28 9:56 AM
What registers do I have to change to decrease the reaction time of the INT2? With this configuration, I have a reaction time of approximately 600ms(When I receive an interrupt in the MCU I read the FUNC_SRC2 to clean the interrupt). I need a reaction time of approximately 100ms. Is possible?
2019-08-29 6:01 AM
Hi,
Found the problem. The problem was that the pin of the INT2 in the MCU have debounce timeout.
Best regards.