LSM303AGR does not seem to store hard iron compensation values I send during configuration
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-03-24 8:16 AM
I've gone through the documentation a few times and I'm not sure what I'm missing. I'm using an STM32L4 to control the lsm303agr through an i2c connection. When I run debug and probe the SCL/SDA lines on my oscilliscope, the messages look good, and from what I am seeing I am getting a slave acknowledge at the end of each transmit.
I first noticed when I was collecting data to calculate hard iron compensation values that after I thought I had sent calibration data to the registers that my collected data looked exactly the same. I made a function to read out the OFFSET registers, and the lsm303agr sends back that all 6 offset registers are 0x00 (seen both in debug and oscilliscope)
Am I getting the procedure to load the compensation data to the registers incorrect?
Magnetometer config registers:
//Magnetometer configuration
//CFG_REG_A_M
msg[0] = CFG_REG_A_M;
msg[1] = 0x88;
HAL_I2C_Master_Transmit(&hi2c1, ACC_ADDR, msg, 2, HAL_MAX_DELAY);
//CFG_REG_B_M
msg[0] = CFG_REG_B_M;
msg[1] = 0x02;
HAL_I2C_Master_Transmit(&hi2c1, ACC_ADDR, msg, 2, HAL_MAX_DELAY);
//CFG_REG_C_M
msg[0] = CFG_REG_C_M;
msg[1] = 0x10;
HAL_I2C_Master_Transmit(&hi2c1, ACC_ADDR, msg, 2, HAL_MAX_DELAY);
sending hard iron values to registers:
//Magnetometer hard-iron compensation values will go here
msg[0] = OFFSET_X_REG_L_M;
msg[1] = 0x7F;
HAL_I2C_Master_Transmit(&hi2c1, ACC_ADDR, msg, 2, HAL_MAX_DELAY);
msg[0] = OFFSET_X_REG_H_M;
msg[1] = 0xFF;
HAL_I2C_Master_Transmit(&hi2c1, ACC_ADDR, msg, 2, HAL_MAX_DELAY);
msg[0] = OFFSET_Y_REG_L_M;
msg[1] = 0xFF;
HAL_I2C_Master_Transmit(&hi2c1, ACC_ADDR, msg, 2, HAL_MAX_DELAY);
msg[0] = OFFSET_Y_REG_H_M;
msg[1] = 0xFF;
HAL_I2C_Master_Transmit(&hi2c1, ACC_ADDR, msg, 2, HAL_MAX_DELAY);
msg[0] = OFFSET_Z_REG_L_M;
msg[1] = 0xD7;
HAL_I2C_Master_Transmit(&hi2c1, ACC_ADDR, msg, 2, HAL_MAX_DELAY);
msg[0] = OFFSET_Z_REG_H_M;
msg[1] = 0xFF;
HAL_I2C_Master_Transmit(&hi2c1, ACC_ADDR, msg, 2, HAL_MAX_DELAY);
and then code when I try to read the values from the registers:
void spitIron(void){
uint8_t reg;
uint8_t data;
reg = OFFSET_X_REG_L_M;
HAL_I2C_Master_Transmit(&hi2c1, MAG_ADDR, ®, 1, HAL_MAX_DELAY);
HAL_I2C_Master_Receive(&hi2c1, MAG_ADDR, &data, 1, HAL_MAX_DELAY);
printf("%s %x \n", "X Low:", data);
reg = OFFSET_X_REG_H_M;
HAL_I2C_Master_Transmit(&hi2c1, MAG_ADDR, ®, 1, HAL_MAX_DELAY);
HAL_I2C_Master_Receive(&hi2c1, MAG_ADDR, &data, 1, HAL_MAX_DELAY);
printf("%s %x \n", "X High:", data);
reg = OFFSET_Y_REG_L_M;
HAL_I2C_Master_Transmit(&hi2c1, MAG_ADDR, ®, 1, HAL_MAX_DELAY);
HAL_I2C_Master_Receive(&hi2c1, MAG_ADDR, &data, 1, HAL_MAX_DELAY);
printf("%s %x \n", "Y Low:", data);
reg = OFFSET_Y_REG_H_M;
HAL_I2C_Master_Transmit(&hi2c1, MAG_ADDR, ®, 1, HAL_MAX_DELAY);
HAL_I2C_Master_Receive(&hi2c1, MAG_ADDR, &data, 1, HAL_MAX_DELAY);
printf("%s %x \n", "Y High:", data);
reg = OFFSET_Z_REG_L_M;
HAL_I2C_Master_Transmit(&hi2c1, MAG_ADDR, ®, 1, HAL_MAX_DELAY);
HAL_I2C_Master_Receive(&hi2c1, MAG_ADDR, &data, 1, HAL_MAX_DELAY);
printf("%s %x \n", "Z Low:", data);
reg = OFFSET_Z_REG_H_M;
HAL_I2C_Master_Transmit(&hi2c1, MAG_ADDR, ®, 1, HAL_MAX_DELAY);
HAL_I2C_Master_Receive(&hi2c1, MAG_ADDR, &data, 1, HAL_MAX_DELAY);
printf("%s %x \n", "Z High:", data);
}//end spitIron
- Labels:
-
I2C
-
STM32L4 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-04-11 5:28 AM - edited 2023-11-20 9:09 AM
Hi @HIngv.1 ,
When you set the magnetometer configuration and hard-iron compensation you use ACC_ADDR instead of MAG_ADDR. Please, try to use MAG_ADDR as described in Table 25 below and let me know if you fix the problem.