2025-01-05 11:25 PM - last edited on 2025-01-08 06:07 PM by Andrew Neil
I have bought a MKI-165V1 to test LPS25HBTR,but I find that the pressure value is decreasing for a long time ,from 1014.117 to 1002.970 in an hour.It is not stable,the next is my initial code,what is the reason for it
2025-01-07 12:05 AM
2025-01-07 10:03 PM
I think this sensor doesn't have many registers, so there's no need to use the official driver. Are there any other reasons for this, or are there any stable sensor configurations you would recommend?
2025-01-08 01:58 AM - edited 2025-01-08 01:58 AM
Hi @2067 ,
It was just a way to check that your fw was correct.
Do you have a reference sensor with which you measure humidity?
2025-01-08 05:51 PM
I am measuring atmospheric pressure with the sensor, and I am currently taking measurements at an altitude of 120 meters indoors. However, without a reference firmware, I have noticed that the sensor readings can vary by more than 10 hPa in the same environment. I would like to know what might be causing this.
2025-01-10 11:35 AM
Hi 2067,
Would it be possible for you to run two identical development boards with your software in the same environment and to compare the results? Can you read sensor's internal temperature?
2025-01-10 05:54 PM
I don't have two boards; I only have one MKI-165V1. This sensor has temperature compensation, and I haven't tried to read the temperature.
How do I use the RPDS registers, and how can I implement the One-Point Calibration feature? Does this chip come with temperature compensation? Can the factory-set parameters affect the output?
2025-01-13 06:54 PM
I don't have two boards; I only have one MKI-165V1. This sensor has temperature compensation, and I haven't tried to read the temperature.
How do I use the RPDS registers, and how can I implement the One-Point Calibration feature? Does this chip come with temperature compensation? Can the factory-set parameters affect the output?