2023-02-17 04:08 AM
Hi
Has nobody used the sensor using SPI interface? I have a power up issue, if CS is left floating till processor drive it to zero it seems device start as i2C and micro Dout is shorted to ground.
Solved! Go to Solution.
2023-02-17 06:22 AM
Welcome, @Community member, to the community!
If you control the LPS22HB via SPI, you should fix CS to GND in your special case via a pull-down of e.g. 10k, so that CS cannot float.
Regards
/Peter
2023-02-17 06:22 AM
Welcome, @Community member, to the community!
If you control the LPS22HB via SPI, you should fix CS to GND in your special case via a pull-down of e.g. 10k, so that CS cannot float.
Regards
/Peter
2023-02-17 06:43 AM
Hi Peter
Thanks for your replay, this fix the problem.
Regards
2023-02-17 07:09 AM
Great!
If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.
Regards
/Peter