2023-07-04 5:30 AM
Hello,
We want to operate the LPS22HB pressure sensor with the i2c protocol. The pin legs of the sensor are connected to the SCL - SDA 4.7k ohm pull-up resistors. Sa0/GND Csi / 3.3 RES / GND. This is how connections are made. This way we can't get data from the sensor. What is the reason of this?
2023-07-04 5:40 AM
2023-07-04 5:40 AM
2023-07-04 5:44 AM
Hello @Legacy member ,
First please make sur that your are using the correct address. You can use an oscilloscope to check SDA and SCL behavior.
Could you share the code ?
Foued
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-07-04 6:29 AM
@Foued_KH Thankk youu <3
All settings are used by default. The code is the library ready code written in arduino. Address 5C and all of its derivatives have been tested by changing the test from within the library. The interrupt pin is not connected anywhere, any problem occurs?
2023-07-05 1:48 AM
2023-07-05 2:53 AM
For I2C communication, 2 pins are required to interface, as this :
VDD to 3.3V DC
SCL to A5
SDA to A4
GND to common groud
Foued
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-07-05 3:14 AM
2023-07-05 7:54 AM
Hi,
The I2C address for LPS22HB is 0xBA or 0xB8 according with SA0 (datasheet page 26).
2023-07-05 8:21 AM
We tried the solutions you suggested but we can't get a solution. Do you have any other suggestions?