cancel
Showing results for 
Search instead for 
Did you mean: 

LIS3MDL does not respond when in Continuous-conversion or Single-conversion mode

TGabo.2
Associate

Hello, I read the Application note AN4602 about the start-up procedure of the LIS3MDL. When I change the mode of the sensor, the DRDY signal remains low and the sensor does not answer to the following I2C transactions.

Without changing the mode of the sensor, I am still able to read the measurement done during the start-up procedure and communicate with I2C with the sensor.

Does anyone had the same issue or has any suggestion?

1 ACCEPTED SOLUTION

Accepted Solutions
TGabo.2
Associate

I suspect an hardware issue on the PCB I am using. I plan to do some tests with a new sensor and PCB.

View solution in original post

3 REPLIES 3
niccolò
ST Employee

Hi @TGabo.2​ ,

did you try to restart the measurment mode after changing modes?

as the AN says, The system goes to idle mode: • automatically at the end of startup procedure

this could be the problem

let me know if this solves it

Niccolò

Eleon BORLINI
ST Employee

Hi @TGabo.2​ ,

do you have any update about your issue?

-Eleon

TGabo.2
Associate

I suspect an hardware issue on the PCB I am using. I plan to do some tests with a new sensor and PCB.